Skip to main content
Visitor II
April 28, 2021
Question

How can i reduce stm32MP1 bootup time further? im expecting to it shoulf boot within 16 sec ?

  • April 28, 2021
  • 1 reply
  • 836 views

systemd-analyze blame:    

 6.297s dev-mmcblk1p3.device

     3.711s user@0.service

     3.668s systemd-udev-trigger.service

      729ms console-kit-log-system-start.service

      663ms weston.service

      598ms systemd-logind.service

      516ms pxl-init-script.service

      489ms lighttpd.service

      373ms systemd-journal-flush.service

      365ms systemd-tmpfiles-setup.service

      348ms sys-kernel-debug.mount

      343ms systemd-journald.service

      339ms dev-mqueue.mount

      312ms systemd-modules-load.service

      308ms tmp.mount

      274ms systemd-update-utmp.service

      238ms systemd-tmpfiles-setup-dev.service

      236ms systemd-remount-fs.service

      236ms kmod-static-nodes.service

      203ms systemd-update-utmp-runlevel.service

      198ms systemd-user-sessions.service

      175ms var-volatile.mount

      175ms sys-kernel-config.mount

      175ms systemd-udevd.service

      152ms sys-fs-fuse-connections.mount

      147ms systemd-sysctl.service

      134ms systemd-random-seed.service

      91ms user-runtime-dir@0.service

      71ms systemd-tmpfiles-clean.service

systemd-analyze :

Startup finished in 3.366s (kernel) + 22.654s (userspace) = 26.021s

multi-user.target reached after 22.049s in userspace

HW info : 

eMMc size if 14.6 GB

rootfs size : 750 MB

Observation :

[13.690249 0.039999] [ OK ] Started Load/Save Random Seed.

[13.866103 0.175854] [ OK ] Started Create Volatile Files and Directories.

[13.923033 0.056930]     Starting Update UTMP about System Boot/Shutdown...

[14.125903 0.202870] [ OK ] Started Update UTMP about System Boot/Shutdown.

[15.832772 1.706869] [  8.767790] galcore: loading out-of-tree module taints kernel.

[15.928784 0.096012] [  8.880145] Galcore version 6.2.4.190076

[16.177606 0.248821] [ OK ] Started udev Coldplug all Devices.

[30.919234 14.741628] [ OK ] Reached target System Initialization.

[30.966229 0.046995] [ OK ] Listening on D-Bus System Message Bus Socket.

[31.051154 0.084926] [ OK ] Listening on dropbear.socket.

[31.067145 0.015990] [ OK ] Reached target Sockets.

[31.099157 0.032012] [ OK ] Reached target Basic System.

[31.147171 0.048014]     Starting Weston Wayland Compositor...

[31.179102 0.031931]     Starting Login Service...

[31.220103 0.041001] [ OK ] Started System Logging Service.

The Bolded line places its taking more time ..

Please help to optimize these time ...

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    April 28, 2021

    Hi, I think you could find some information in https://wiki.st.com/stm32mpu/wiki/How_to_optimize_the_boot_time

    Regards.