How can I use tamper pins as a wakeup source?
Hi, I am looking all through the wiki, but I do not see any clue on using the tampers as a wakeup source.
How can I configure the tampers to wake up the stm32mp1 from low power modes?
Is it posible to wake up from VBAT? Or is VBAT only a energy mode to maintain the data in the memories? Can I run a piece of code in VBAT mode? If so, how could I do it? What restrictions do apply?
When I say a piece of code, I mean it can be baremetal or linux or whatever it can run.
Best regards,
Andrés