How can the MP1 M4 Core be woken up by an LPTimer in STOP mode?
I have built a test program from the two examples PWR_STOP_CoPro and LPTIM_PulseCounter. With the LPTIM_PulseCounter I changed the CounterSource to LPTIM_COUNTERSOURCE_INTERNAL and adjusted the priority HAL_NVIC_SetPriority (LPTIM2_IRQn, 0, 0);
Both programs run as expected only when I start the timer HAL_LPTIM_TimeOut_Start_IT (& hlptim2, 0xFFFF, 0x7000) and then go to STOP Mode HAL_PWR_EnterSTOPMode (PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI); the M4 core does not wake up by the LP Timer interrupt, but an EXTI interrupt lets it wake up.
Can someone tell me what I might have overlooked?