How to connect adc driver in dts with libiio - stm32mp1
Hi,
I try to connect ADC channels with libiio for my custom board based on the stm32mp157caa3. I followed the instructions from the link
https://wiki.st.com/stm32mpu/wiki/IIO_libiio
https://wiki.st.com/stm32mpu/wiki/ADC_device_tree_configuration#DT_configuration_examples
but without success. After issuing the console
iio_infoI get
Library version: 0.23 (git tag: 92d6a35)
Compiled with backends: local xml ip usb serial
IIO context created with local backend.
Backend version: 0.23 (git tag: 92d6a35)
Backend description string: Linux stm32mp1-connect-bridge 5.15.67 #1 SMP PREEMPT Thu Sep 8 10:32:54 UTC 2022 armv7l
IIO context has 2 attributes:
local,kernel: 5.15.67
uri: local:
IIO context has 0 devices:The same is in
/sys/bus/iio/devices/empty, with no devices.
Part of my dts looks
&adc{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&adc_pins_mx>;
pinctrl-1 = <&adc_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN adc */
vdda-supply = <&vdda>; /* Example to supply vdda pin by using a PMIC regulator */
vref-supply = <&vrefbuf>; /* Example to use VREFBUF (It needs to be enabled as well) */
adc1: adc@0 {
assigned-resolution-bits = <12>;
/* Single-ended channels */
channel@0 {
reg = <0>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@1 {
reg = <1>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@2 {
reg = <2>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@3 {
reg = <3>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@5 {
reg = <5>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@6 {
reg = <6>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@9 {
reg = <9>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@10 {
reg = <10>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@12 {
reg = <12>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@13 {
reg = <13>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@15 {
reg = <15>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@17 {
reg = <17>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
};
/* USER CODE END adc */
};In the Kernel configuration, I also marked
Device Drivers --->
<*> Industrial I/O support --->
Analog to digital converters --->
<*> STMicroelectronics STM32 adc core
<*> STMicroelectronics STM32 adcIt must be something I missed.
Thanks in advance for the hints.
BR Michal