Skip to main content
Visitor II
January 29, 2021
Question

How to control GPIO using DT in Application?

  • January 29, 2021
  • 2 replies
  • 840 views

I want to control defined GPIO in DT in Applicatoin code.

But I can't control this, please let me know how to control gpio with DT in applicatoin.

1) I can control GPIO in Application without DT . (unused at gpioinfo)

2) I can't control GPIO in application with DT, like below.

  • gpioinfo​

  line 14:   unnamed "stm32mp:green:user" output active-low [used]

​ occurred error massage when running application code

Failed to issue GET LINEHANDLE IOCTL (-25)

Failed to issue GPIOHANDLE_SET_LINE_VALUES_IOCTL (-25)

Failed to issue GPIOHANDLE_SET_LINE_VALUES_IOCTL (-25)

Failed to issue GPIOHANDLE_SET_LINE_VALUES_IOCTL (-25)

reference code

https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace

Device Tree - add green led

led {

compatible = "gpio-leds";

blue {

label = "heartbeat";

gpios = <&gpiod 9 GPIO_ACTIVE_HIGH>;

linux,default-trigger = "heartbeat";

default-state = "off";

};

green {

label = "stm32mp:green:user";

gpios = <&gpioa 14 GPIO_ACTIVE_LOW>;

default-state = "on";

};

};

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    February 1, 2021

    ​Hello BKwak.1 (Community Member),

    You should care not to mix user space and kernel space. Either you control the GPIO in user space using gpiolib,  like it is specified in:https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace

    or you modify the DT and you control the GPIO in kernel space.

    https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_kernel_space

    For the specific gpio-leds driver, you can refer to

    https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package

    Regards,

    Olivier

    Visitor II
    March 18, 2021

    Hi, so to be clear - Is there in fact no way to enable a pull-down at the low level, like (preferably) u-boot or kernel device tree, but then be able to control the GPIO from user space as we are now? We forgot an external pull down to a FET and would prefer not to rework it if possible.