How to disable PMIC from powering up when USB cable is inserted.
Currently our custom board powers up in two cases, one when you press the power on button, and another when you plug in the USB cable.
We would like to disable PMIC from powering on when USB cable is plugged in. We see that the STPMIC specification document (section 5.4.2), lists the three conditions which triggers PMIC turn-on and also the register bit VBUSOTG_DET_DIS which needs to be set to 1 to disable this feature.
Since I cannot write to PMIC register address 0x40, was wondering if there is any device tree setting which sets this bit?
Any information on how to do this would be very much appreciated.
Thanks!