Skip to main content
Visitor II
September 29, 2020
Question

How to display splash screen on HDMI monitor?

  • September 29, 2020
  • 1 reply
  • 1309 views

Hi i want to display splash screen on HDMI monitor instead of DSI monitor of STM32MP157C-DK2. I know that it has something to do with U-Boot configuration, but i can't find right options to enable this feature. I would be grateful if somebody could help me.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    September 29, 2020

    Hi @La​ 

    Guess this page might help https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI

    Olivier

    La1Author
    Visitor II
    September 30, 2020

    Hi, thanks for answer, but i have not found useful information there. They only say that "The U-Boot graphical console ("ST life.augmented" picture) is never displayed on the HDMI monitor. This console is displayed on the DSI display (if any on the board).", but i assume, that it is only on default starter package and it can be changed using developer or distribution package. On page https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#U-Boot_description they say that U-Boot supports "Display: LCD, HDMI, BMP for splashcreen", so i think it should be possible.