How to safely create a DDR definition file for HAL?
I've inherited a board that is based on an STM32MP135AAE3 and has an external DDR (W63AH6NBVABI, a DRAM 1Gb LPDDR3 from Winbond). It appears I need to create a DDR.h file similar to the stm32mp13xx-ddr3-4Gb.h or stm32mp13xx-ddr3-8Gb.h files that STM provides (right?)
I've taken the existing stm32mp13xx-ddr3-4Gb.h and am slowly going through, figuring out exactly what each line needs and then trying to track down the appropriate information from the DDR datasheet. My biggest concern is that I get the timing ALMOST right and end up with a DDR that works 99.99% of the time (failing, of course, only at customer sites).
1) Is there an archive of DDR definition files somewhere that I missed?
2) Is there a better way to generate this DDR definition file?
3) Is there a way to test I did it right besides running various memory tests for days and days?
As an example, this file needs information like this:
// DDRCTRL SDRAM timing register 0
/*
Name Bits Meaning
---- ---- -------
WR2PRE 30:24 Minimum time between write and precharge to same bank
T_FAW 21:16 tFAW Valid only when 8 or more banks(or banks x bank groups) are present.
In 8-bank design, at most 4 banks must be activated in a rolling window
of tFAW cycles.
T_RAS_MAX 14:8 Maximum time between activate and precharge to same bank
T_RAS_MIN 5:0 Minimum time between activate and precharge to the same bank.
*/