How to solve target detection problem?
I have a STM32MP157A-DK1 board. I can't connect to it via ST-Link Utility. It says the target is not detected. Although if I select "Firmware Update" from ST-LINK menu, it updates the firmware of the board (the red-green led blinks etc). But can't connect otherwise.
I tried moving the BOOT0 and BOOT2 pins on-off in every combination, tried inserting and removing the SD Card, plugging and unplugging the USB-C power cable. I have installed all ST-Link drivers and reinstalled them, etc, etc... I even tried all the possible options at the target settings screen, but to no avail. Can anyone offer me a solution?