I have compiled the stm32mp157 disco V2.0.0.0 Distribution package for both the x11 (matchbox desktop) and the x11-xfce image, insuring that I accept the EULA. When I run both images, response times and memory image are very large compared to V1.2
I have xfce running very well in the V1.2 Yocto Distribution system on the stm32mp157c disco board. The xfce desktop is very responsive and uses about 100M of memory. The xfce desktop using the latest V2.0.0 Distribution image however is very sluggish and even a simple mouse movement will cause near 100% cpu utilization. Memory usage is around 200M or more with the Xorg server alone using up 16M of memory. It would appear that the new image is not accelerated. I see similar behavior with the x11 image (matchbox desktop) so the issue is not the desktop but with the underlying system. Is there something setup parameter I am missing? I also noted that the weston image seems to run fine!