I just received STM32MP157F-EV1. On boot, the LCD displays nothing and the onboard ST-Link will not properly enumerate (Windows says "USB Device Not Recognized"). Latest ST-Link driver is installed and working with other kits. Is this a faulty board?
The ST-Link LEDs are very dimly lit when powered...they are much brighter on my STM32MP157F-DK2 board. I suspect some hardware problem with the MPU board. Also, the CPU LEDs do appear to be running (the Linux Blue LED blinks after a while, and with the SD Card removed the Red LED blinks as in DFU mode). Just not sure why there is no display (no backlight) and no ST-Link function.