Skip to main content
Visitor II
December 15, 2020
Solved

I'm wondering what's the difference point between STM32MP157C-DK2 and STM32MP157F-DK2?

  • December 15, 2020
  • 2 replies
  • 1283 views

Hi.

I was going to buy STM32MP157C-DK2 but its status NRND(Not Recommended for New Design). So I think to buy STM32MP157F-DK2.

Are they different point is only a clock(650 or 800) of A7 core? What's the difference?

Thank you.

Best regards.

    This topic has been closed for replies.
    Best answer by PatrickF

    I confirm that the major differences are the increased max frequency of the Cortex-A7 cores and the corrections of some HW bugs (Device Rev.Z, see ES0438).

    2 replies

    Technical Moderator
    December 15, 2020

    Hi @Jungho​ ,

    STM32MP157F-DK2 is assembled with latest STM32MP15 RevZ cut which is the only one available for new product now.

    Olivier

    PatrickFAnswer
    Technical Moderator
    December 16, 2020

    I confirm that the major differences are the increased max frequency of the Cortex-A7 cores and the corrections of some HW bugs (Device Rev.Z, see ES0438).