Skip to main content
Graduate
October 4, 2021
Solved

Increase VRING_SIZE from 16 to 32 in both processors

  • October 4, 2021
  • 4 replies
  • 2005 views

Hi there,

I am writing an application that requires large streams of IPCC. At the moment I have allocated the RPMSG vdev0 and vrings to SRAM3+4 and I have increased the buffer size of each ring to 1024.

The device tree now looks like this:

 vdev0vring0: vdev0vring0@10040000 {
			compatible = "shared-dma-pool";
			reg = <0x10040000 0x2000>;
			no-map;
		};
 
		vdev0vring1: vdev0vring1@10042000 {
			compatible = "shared-dma-pool";
			reg = <0x10042000 0x2000>;
			no-map;
		};
 
		vdev0buffer: vdev0buffer@10044000 {
			compatible = "shared-dma-pool";
			reg = <0x10044000 0x8000>;
			no-map;
		};

On the M4 Linker Script:

RAM2_ipc_shm		(xrw)	: ORIGIN = 0x10040000,	LENGTH = 0x00012000 

I am trying to increase the VRING_SIZE to more than 16 ( Ideally I would like to increase it to maximum possible value in my configuration). In Openapm_conf:

 #VRING_NUM_BUFFS 16

I have increased the memory in my device tree but I can not find the remoteproc config declaration for VRING size on linux side. Based on this article I assume that I have to increase the VRING_SIZE in both the rproc linux config and the openamp_conf in the M4. If there are any ides on how to configure VRING_SIZE on the linux side would be highly appreciated.

    This topic has been closed for replies.
    Best answer by Kevin HUBER

    Hi @KChar.1​ ,

    I would like to know, why you want to increase the number of vring buffer and why you do not just increase the size of the buffer, like in your previous post? https://community.st.com/s/question/0D53W00000qwjyiSAA/increased-1024-rpmsg-buffer-size-will-fail-on-mailbox-vdev-declaration

    Anyway, I was able to realize the modification on my stm32mp157f-dk2 board with success, by increasing the VRING_NUM_BUFFS from 16 to 32.

    You only need to modify the define in openamp_conf.h

    #define VRING_NUM_BUFFS 32		 /* number of rpmsg buffer */

    Then the modifications will be propagated to the linux automatically, thanks to the shared resource table. Defined in rsc_table.c in M4.

    CONST struct shared_resource_table __resource __attribute__((used)) resource_table = {
    	/* Vring rsc entry - part of vdev rsc entry */
    	.vring0 = {VRING_TX_ADDRESS, VRING_ALIGNMENT, VRING_NUM_BUFFS, VRING0_ID, 0},
    	.vring1 = {VRING_RX_ADDRESS, VRING_ALIGNMENT, VRING_NUM_BUFFS, VRING1_ID, 0},

    On linux side, when the driver virtio is probed, it will get its information from the shared resource table, previously filled by the M4 core.

    This is done inside the file drivers/virtio/virtio_ring.c

    On M4 side, remember to increase the area in the dts. This is my configuration with 32 buffers of 512 bytes :

    		vdev0vring0:vdev0vring0@10040000{
    			compatible = "shared-dma-pool";
    			reg = <0x10040000 0x2000>;
    			no-map;
    		};
     
    		vdev0vring1:vdev0vring1@10042000{
    			compatible = "shared-dma-pool";
    			reg = <0x10042000 0x2000>;
    			no-map;
    		};
     
    		vdev0buffer:vdev0buffer@10044000{
    			compatible = "shared-dma-pool";
    			reg = <0x10044000 0x8000>;
    			no-map;
    		};

    In your case, since you increased the size of the buffers from 512 to 1024, please update the dts accordingly.

    Then the final modifications is the linker file of M4. Where the ipc area length must be equal to the three areas defined in the dts.

    In my case 0x2000 + 0x2000 + 0x8000 = 0xA000, but modify it regarding your dts.

     RAM2_ipc_shm		(xrw)	: ORIGIN = 0x10040000,	LENGTH = 0x0000A000

     And it should works!

    Now you can verify your modifications thanks to /sys/kernel/debug.

    Once your board boots, you can:

    cat /sys/kernel/debug/remoteproc/remoteproc0/resource_table

    To verify that you allocated 32 buffers for each side RX/TX

     Number of buffers 32

    You can also checks the area that you defined inside the DTS by using:

    cat /sys/kernel/debug/remoteproc/remoteproc0/carveout_memories

    In my case:

    Carveout memory entry:
     Name: vdev0vring0
     Virtual address: f8b4a303
     DMA address: 0x10040000
     Device address: 0x10040000
     Length: 0x2000 Bytes
     
    Carveout memory entry:
     Name: vdev0vring1
     Virtual address: 135e15b0
     DMA address: 0x10042000
     Device address: 0x10042000
     Length: 0x2000 Bytes
     
    Carveout memory entry:
     Name: vdev0buffer
     Virtual address: 00000000
     DMA address: 0x00000000
     Device address: 0x10044000
     Length: 0x8000 Bytes

    These two files are very helpful to debug and verify that everything is correct on your board.

    Regards,

    Kevin

    In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

    4 replies

    Technical Moderator
    October 20, 2021

    Hello @KChar.1​ ,

    Sorry for the late reply.

    Did you succeed to increase the Vring size or find another way to make your application works?

    Regards,

    Kévin

    KChar.1Author
    Graduate
    October 20, 2021

    Hi @Kevin HUBER​ ,

    Thanks for getting back to me. Unfortunately I have not find a way to increase the VRING size yet. With my current linux image and device tree I can modify the VRING size on the M4 side (openamp_conf.h) to any value up to 16. When I attempt values above 16 I can not send or receive through IPCC. My assumption at the moment is that I have to allocate more memory in the linux kernel and specify my desired VRING size there, but I can not find exactly in which kernel object I have to do this adjustment.

    Any advice would be really appreciated.

    Regards,

    Kyr

    Technical Moderator
    October 22, 2021

    Hi @KChar.1​ ,

    I would like to know, why you want to increase the number of vring buffer and why you do not just increase the size of the buffer, like in your previous post? https://community.st.com/s/question/0D53W00000qwjyiSAA/increased-1024-rpmsg-buffer-size-will-fail-on-mailbox-vdev-declaration

    Anyway, I was able to realize the modification on my stm32mp157f-dk2 board with success, by increasing the VRING_NUM_BUFFS from 16 to 32.

    You only need to modify the define in openamp_conf.h

    #define VRING_NUM_BUFFS 32		 /* number of rpmsg buffer */

    Then the modifications will be propagated to the linux automatically, thanks to the shared resource table. Defined in rsc_table.c in M4.

    CONST struct shared_resource_table __resource __attribute__((used)) resource_table = {
    	/* Vring rsc entry - part of vdev rsc entry */
    	.vring0 = {VRING_TX_ADDRESS, VRING_ALIGNMENT, VRING_NUM_BUFFS, VRING0_ID, 0},
    	.vring1 = {VRING_RX_ADDRESS, VRING_ALIGNMENT, VRING_NUM_BUFFS, VRING1_ID, 0},

    On linux side, when the driver virtio is probed, it will get its information from the shared resource table, previously filled by the M4 core.

    This is done inside the file drivers/virtio/virtio_ring.c

    On M4 side, remember to increase the area in the dts. This is my configuration with 32 buffers of 512 bytes :

    		vdev0vring0:vdev0vring0@10040000{
    			compatible = "shared-dma-pool";
    			reg = <0x10040000 0x2000>;
    			no-map;
    		};
     
    		vdev0vring1:vdev0vring1@10042000{
    			compatible = "shared-dma-pool";
    			reg = <0x10042000 0x2000>;
    			no-map;
    		};
     
    		vdev0buffer:vdev0buffer@10044000{
    			compatible = "shared-dma-pool";
    			reg = <0x10044000 0x8000>;
    			no-map;
    		};

    In your case, since you increased the size of the buffers from 512 to 1024, please update the dts accordingly.

    Then the final modifications is the linker file of M4. Where the ipc area length must be equal to the three areas defined in the dts.

    In my case 0x2000 + 0x2000 + 0x8000 = 0xA000, but modify it regarding your dts.

     RAM2_ipc_shm		(xrw)	: ORIGIN = 0x10040000,	LENGTH = 0x0000A000

     And it should works!

    Now you can verify your modifications thanks to /sys/kernel/debug.

    Once your board boots, you can:

    cat /sys/kernel/debug/remoteproc/remoteproc0/resource_table

    To verify that you allocated 32 buffers for each side RX/TX

     Number of buffers 32

    You can also checks the area that you defined inside the DTS by using:

    cat /sys/kernel/debug/remoteproc/remoteproc0/carveout_memories

    In my case:

    Carveout memory entry:
     Name: vdev0vring0
     Virtual address: f8b4a303
     DMA address: 0x10040000
     Device address: 0x10040000
     Length: 0x2000 Bytes
     
    Carveout memory entry:
     Name: vdev0vring1
     Virtual address: 135e15b0
     DMA address: 0x10042000
     Device address: 0x10042000
     Length: 0x2000 Bytes
     
    Carveout memory entry:
     Name: vdev0buffer
     Virtual address: 00000000
     DMA address: 0x00000000
     Device address: 0x10044000
     Length: 0x8000 Bytes

    These two files are very helpful to debug and verify that everything is correct on your board.

    Regards,

    Kevin

    In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

    KChar.1Author
    Graduate
    October 26, 2021

    Hi @Kevin HUBER​,

    Thanks a lot for the detailed explanation! I tested successfully your example with 1024 buffer size and 32 VRINGS. I was missing the right alignment on the M4 linker script in previous attempts.

    I am using a user-space application that has to send a big amount of data. Each string that leaves from A7 could be up to 1024 bytes (but most strings are aprox 128 bytes) This was the reason I already increased the buffer size in 1024 as in the previous posts. The A7 application is based on a clock that depending on user action can send multiple strings (up to 128) to the remote_proc[M4]. If the amount of strings is bigger than the VRING size then the application will hang until the message is processed by the M4 as expected. This is why I would like to increase the VRING size in the first place and try to find a workaround for these large IPCCs.

    The debugging files are a huge help too! Thanks again for this!

    Regards,

    Kyr