Skip to main content
Visitor II
December 2, 2022
Question

Installing Distribution package for 1st time.

  • December 2, 2022
  • 1 reply
  • 887 views

Hi,

I was downloading and installing Distribution package for the 1st time following this link: https://wiki.st.com/stm32mpu-ecosystem-v3/wiki/STM32MP1_Distribution_Package

As I want version openstlinux-5.10-dunfell-mp1-21-03-31

After source sync there are no files present. May I know why its discarding?

root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31# repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.10-dunfell-mp1-21-03-31

.repo/manifests/: discarding 3 commits

Your identity is: ***.*** [removed by moderator]

If you want to change this, please re-run 'repo init' with --config-name

Testing colorized output (for 'repo diff', 'repo status'):

 black  red   green  yellow  blue   magenta  cyan   white

 bold   dim   ul    reverse

Enable color display in this user account (y/N)?

repo has been initialized in /

If this is not the directory in which you want to initialize repo, please run:

  rm -r //.repo

and try again.

root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31# repo sync

Fetching project openembedded-core

Fetching projects: 12% (1/8)

Fetching project meta-openembedded

Fetching projects: 25% (2/8)

Fetching project bitbake

Fetching projects: 37% (3/8)

Fetching project meta-st-openstlinux

Fetching projects: 50% (4/8)

Fetching project meta-st-stm32mp

Fetching projects: 62% (5/8)

Fetching project meta-qt5/meta-qt5

Fetching projects: 75% (6/8)

Fetching project meta-st-scripts

Fetching projects: 87% (7/8)

Fetching project meta-st-stm32mp-addons

Fetching projects: 100% (8/8)

Fetching projects: 100% (8/8), done.

Syncing work tree: 100% (8/8), done.

layers/meta-openembedded/: discarding 137 commits

layers/meta-qt5/: discarding 6 commits

layers/meta-st/meta-st-openstlinux/: discarding 24 commits

layers/meta-st/meta-st-stm32mp/: discarding 36 commits

layers/meta-st/meta-st-stm32mp-addons/: discarding 4 commits

layers/meta-st/scripts/: discarding 2 commits

layers/openembedded-core/: discarding 587 commits

layers/openembedded-core/bitbake/: discarding 23 commits

root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31# ls

root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31#

Thankyou

    This topic has been closed for replies.

    1 reply

    ST Employee
    December 20, 2022

    Hello,

    I recommend you to use the latest version of the distribution package.

    Regards,

    Grégory