Interfacing external uart peripheral with STM32MPUDK2
I have stm32mpdk2 board and trying to interface a uart based peripheral ( nfc) .I have connected Tx , RX , Vdd, GND > pin (12,8,1,6) .
tty driver is already enabled in the kernel. and the peripheral on powering up shows the init sequence correctly(led pattern is correct)
below are the logs for dmesg | grep tty*
[ 0.000000] Kernel command line: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200
[ 1.702933] 4000e000.serial: ttySTM3 at MMIO 0x4000e000 (irq = 53, base_baud = 4000000) is a stm32-usart
[ 1.703246] serial serial0: tty port ttySTM3 registered
[ 1.704628] 40010000.serial: ttySTM0 at MMIO 0x40010000 (irq = 54, base_baud = 4000000) is a stm32-usart
[ 2.915213] printk: console [ttySTM0] enabled
[ 7.768477] systemd[1]: Unnecessary job for /dev/ttySTM0 was removed.
[ 7.781958] systemd[1]: Created slice system-getty.slice.
[ 7.817838] systemd[1]: Created slice system-serial\x2dgetty.slice.
But I cant seem to find teh correct tty for this perihperal.
Same logs comes even if I remove the device
plz advice the changes or any example for external uart perihperal interfacing
Br,