Skip to main content
Explorer
July 16, 2021
Solved

Is boards not recommended for new design? STM32MP157C-DK1 STM32MP157C-DK2

  • July 16, 2021
  • 3 replies
  • 810 views

I am looking for STM32MP157A-DK1 and STM32MP157A-DK2 Why thouse boards is not recommended for new design? Which developer board you can recommend?

@PatrickF​ @Community member​ @SEam72​ 

    This topic has been closed for replies.
    Best answer by PatrickF

    Hi,

    These boards has been replaced by new boards using faster 800MHz processor. They are 100% backward compatible with previous one (same HW, same SW).

    STM32MP157A-DK1 and STM32MP157C-DK2 has been replaced respectively by STM32MP157D-DK1 and STM32MP157F-DK2

    Note that all the 650MHz devices versions still exist with the 10-year longevity program (as well the 800MHz versions), just the 650MHz boards has been discontinued (800MHz boards cover as well the 650MHz evaluation purposes)

    Regards.

    3 replies

    PatrickFAnswer
    Technical Moderator
    July 16, 2021

    Hi,

    These boards has been replaced by new boards using faster 800MHz processor. They are 100% backward compatible with previous one (same HW, same SW).

    STM32MP157A-DK1 and STM32MP157C-DK2 has been replaced respectively by STM32MP157D-DK1 and STM32MP157F-DK2

    Note that all the 650MHz devices versions still exist with the 10-year longevity program (as well the 800MHz versions), just the 650MHz boards has been discontinued (800MHz boards cover as well the 650MHz evaluation purposes)

    Regards.

    Technical Moderator
    July 16, 2021

    You can use the successor boards STM32MP157D-DK1 and STM32MP157F-DK2.

    Good luck!

    /Peter

    Technical Moderator
    July 16, 2021

    In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'