Is it possible to achieve an ADC sampling rate of 500ksps and more via the iio interface, and if yes, how?
Hi all,
I followed the instructions described on the wiki, page ADC_device_tree_configuration.
Changing the sampling_frequency, I can achieve a sampling rate of about 10k. Going higher crashes the system.
Reducing the parameter 'min-sample-time-nsecs' in the device tree did not solve the issue.
Is it not possible to go higher with the sampling rate when using the iio interface? Would I option higher sampling rates writing a C Program accessing the ADC via mmap()?
Any hint is appreciated.
Denise