Skip to main content
Visitor II
June 22, 2022
Question

Is it possible to connect an IMX477 on the STM32MPU157F-dk2

  • June 22, 2022
  • 2 replies
  • 1479 views

Hello,

When I plugged the IMX477 on a USB port and I have the following msg:

[ 7307.355686] usb 2-1.3: new high-speed USB device number 5 using ehci-platform

[ 7307.519593] uvcvideo: Found UVC 1.00 device Arducam IMX477 HQ Camera (0c45:636d)

[ 7307.534627] input: Arducam IMX477 HQ Camera: Arduc as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.3/2-1.5

[ 7307.550269] usb 2-1.3: 3:1: cannot get freq at ep 0x84

[ 7308.295030] usb 2-1.3: 3:1: cannot get freq at ep 0x84

[ 7308.349280] usb 2-1.3: 3:1: cannot get freq at ep 0x84

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    July 11, 2022

    Hi @JACQUES Jérôme​ ,

    I'm not expert but I understand that such device may require some specific driver/support which does not looks to be by default in OpenSTLinux.

    Which version of ecosystem are you using ?

    Olivier

    JJérô.1Author
    Visitor II
    July 11, 2022
    Hello,
    another question, issu it possible to connect the amicam1 with the stm32MPU157f-dk2?
    Thanks a lot,
    Jérôme
    JJérô.1Author
    Visitor II
    July 11, 2022

    Hi Olivier,

    Thanks for you interest !

    I'm using the 2.1. I see there is the 4.0 version maybe ....

    A question Olivier, do you work in Sophia Antipolis ?

    If yes, is it possible to have a meeting ?

    Best regards,

    Jérôme