Skip to main content
Visitor II
August 29, 2019
Question

Is it possible to install Raspbian on the STM32MP1 ? This is in order for example to interface the FLIR Lepton with it.

  • August 29, 2019
  • 1 reply
  • 795 views

See here

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    September 2, 2019

    ​Hello RogerPaudex (Flybotix),

    At this time we only support our own OpenSTLinux s/w distribution, therefore at present Raspbian won't run on the STM32MP1as is.

    You will need to customize your project to interface with the FLIR camera sensor, to interface with the SPI and I2C ports (STM32CubeMx can do that, in addition with the device tree generation) as well as application examples in STM32Cube_FW_MP1 library for SPI and I2C use.

    I hope it helps.

    Best Regards,

    Olivier