Skip to main content
Graduate
May 31, 2024
Solved

Is it possible to make this system using stm32mp157??

  • May 31, 2024
  • 1 reply
  • 1182 views

Hello,

I would like to make the system below using stm32mp157.

- System Description -

1. 100Mbps Full-Duplex Ethernet

2. Cortex-A7 receives and transmits data from Ethernet on the PC. 

3. Cortex-A7 calculates Ethernet data and sends the result to Cortex-M4.

4. Cortex-M4 controls peripheral(SPI, I2C, UART, GPIO) using DMA and interrupt 

 

Can I implement a program like the above??

I've usually used F4 series or L4 series, so I don't know about MPU lines.

If the program is implementable, please let me know what I need to know.

If the program cannot be implemented, please recommend MCU or method that can be implemented.

 

    This topic has been closed for replies.
    Best answer by Jean-Christophe_TROTIN

    Hi @inkong,

     

    I think that the system that you described is possible with the STM32MP157 lines.

    As you said that you “don’t know about MPU lines”, I could suggest that you have a look at the STM32 MPU wiki (https://wiki.st.com/stm32mpu/wiki/Main_Page), if you don’t know it yet.

     

    The following articles might be interesting for you:

    Hope this information helps.

     

    Regards,

    JC.

    1 reply

    ST Employee
    June 4, 2024

    Hi @inkong,

     

    I think that the system that you described is possible with the STM32MP157 lines.

    As you said that you “don’t know about MPU lines”, I could suggest that you have a look at the STM32 MPU wiki (https://wiki.st.com/stm32mpu/wiki/Main_Page), if you don’t know it yet.

     

    The following articles might be interesting for you:

    Hope this information helps.

     

    Regards,

    JC.

    inkongAuthor
    Graduate
    June 5, 2024

    Hi Jean,

     

    Thank you for your kind reply!! :)

    I'll refer to the article you attached.

     

    Sincerely,

    inkong.