Is it possible to power the board without using the USB-C ?
On the STM32MP157-DK1 schematic there is a note to say "WARNING - do not supply 3V3,5V from Arduino shield", even though it looks as though pin 5 on CN16 is electrically connected to 5V_VIN via a 0R resistor.
It's going to be very inconvenient to use the USB-C connector from within an enclosure , so I was wondering if that was just because the board wants more power than a single pin can provide ? Or if there's another reason.
There is no such note on the GPIO Expansion header (where pins 2,4 are connected to 5V_IN) - is this because there are 2 pins to share the load, or should I not power the board from the GPIO expansion header either ?