Skip to main content
Graduate
September 19, 2021
Question

Is my stm32mp157c-dk2 board bricked?

  • September 19, 2021
  • 1 reply
  • 1100 views

Hello,

I don't know what happened but suddenly on putting the board in boot mode( boot switches ON) , I cant detect the board on the stm32cube programmer and I see a green led ( PWR_IN) continuously blinking!

attached is the image.

Please assist.

Br,

D

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    September 20, 2021

    Hi,

    LD2 is 5V presence, so, if blinking, it is likely the current limitation inside your USB Type-C supply (I assume blinking rate is very slow).

    Did you try another USB Type-C supply/cable ?

    Regards.

    darla14Author
    Graduate
    September 23, 2021

    @PatrickF​ Thanks for the reply, Yes I did try another C type USB as well as the USB PD adapter. But same response.

    Is there any IC that I have blown up and which could be causing this?

    Please advice.

    I have access to lab where I have soldering accessories.

    Br,

    D

    Graduate II
    September 23, 2021

    >>Is there any IC that I have blown up and which could be causing this?

    Could be any of a number of parts.

    Could you have causes an ESD event when you fiddled with the switches?

    Placed the board on a conductive surface?

    Pull a schematic and start double checking supply rails, etc.

    What if you remove the SD card?