Skip to main content
Visitor II
October 8, 2019
Question

is start the weston services must have the gpu support

  • October 8, 2019
  • 1 reply
  • 916 views

is stm32mp153 can start weston without gpu

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    October 8, 2019

    Hi @Jzhua​ 

    Yes OpenSTLinux Weston can be used without GPU.

    Using Distribution package if you reject the GCNANO licence agreement during configuration, you will have an automatic fallback to Weston display path not using GPU.

    Hope it help

    Olivier

    JzhuaAuthor
    Visitor II
    October 9, 2019

    I just see the need to accept the eula. Do I need to say no? Like this

    Do you accept the EULA you just read? (y/n) n
    [WARNING] Configure build without support of packages under EULA acceptance.

    Technical Moderator
    October 10, 2019

    Yes that's it.

    Note that further adaptation may have to be done in the boot chain and Kernel Device Tree.

    Using STM32CubeMX is recommended to help writing them.

    Olivier