Skip to main content
Visitor II
December 8, 2022
Question

Is there any STM MCU/MPU which can be used for computer vision applications

  • December 8, 2022
  • 2 replies
  • 945 views

Is there any STM MCU/MPU which can be used for computer vision applications such as face recognition, Object detection/tracking? If so, how much flash memory required to process video with 5MP camera at 30FPS?

Is there any STM MCU/MPU which can be used for AR/VR applications?

    This topic has been closed for replies.

    2 replies

    Super User
    December 9, 2022

    The STM32MP series is more suited. But even more suited would be a full blown computer.

    5MP * 30fps * 3bpp = 3.6 GBps. Not processing that on an MCU.

    Technical Moderator
    January 6, 2023

    Hi @NPete.3​ 

    please have a look to https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_OpenSTLinux_Expansion_Package

    and more specifically https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_-_face_recognition_using_TensorFlow_Lite_C%2B%2B_API

    Regards,

    In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'