Issue regarding registers of USBPHYC in STM32MP157A with Linux(V5.13)
Hello,
I am working on a custom board based on STM32MP157A . For USBPHYC i am referring the driver from Linux(V5.13) and some of the registers like STM32_USBPHYC_MONITOR mentioned in the driver file are missing in the reference manual (RM0436).So i just wanted to know is it the only register missing in the reference manual (or) are there any other registers missing .If yes, could you help me in finding those registers with their offset addresses and their functionality or suggest me the actual reference manual.
please find the below attached link for the driver file i am using :
https://elixir.bootlin.com/linux/v5.13/source/drivers/phy/st/phy-stm32-usbphyc.c
Thanks&Regards,
Srikanth.