Issue with otm8009a mipi dsi panel configuration on the stm32mp157c-odyssey
Hello. I'm trying to configure the otm8009a 800x480 display panel from the stm32mp157f-dk2 dev kit on the Seeed Studio's stm32mp157c-odyssey board.
The issue is that by probing display with modetest -M stm I'm getting:
failed to open device 'stm': No such file or directoryBut with modetest -M simpledrm I'm getting this output:
Encoders:
id crtc type possible crtcs possible clones
34 0 none 0x00000001 0x00000001
Connectors:
id encoder status name size (mm) modes encoders
35 0 connected Unknown-1 127x211 1 34
modes:
index name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot
#0 480x800 60.00 480 480 480 480 800 800 800 800 23040 flags: ; type: preferred, driver
props:
1 EDID:
flags: immutable blob
blobs:
value:
2 DPMS:
flags: enum
enums: On=0 Standby=1 Suspend=2 Off=3
value: 3
5 link-status:
flags: enum
enums: Good=0 Bad=1
value: 0
6 non-desktop:
flags: immutable range
values: 0 1
value: 0
4 TILE:
flags: immutable blob
blobs:
value:
CRTCs:
id fb pos size
33 0 (0,0) (0x0)
#0 nan 0 0 0 0 0 0 0 0 0 flags: ; type:
props:
24 VRR_ENABLED:
flags: range
values: 0 1
value: 0
Planes:
id crtc fb CRTC x,y x,y gamma size possible crtcs
31 0 0 0,0 0,0 0 0x00000001
formats: RG16 XR24
props:
8 type:
flags: immutable enum
enums: Overlay=0 Primary=1 Cursor=2
value: 1
30 IN_FORMATS:
flags: immutable blob
blobs:
value:
01000000000000000200000018000000
01000000200000005247313658523234
03000000000000000000000000000000
0000000000000000
in_formats blob decoded:
RG16: LINEAR
XR24: LINEAR
Frame buffers:
id size pitchSo display is actually working with simpledrm and I am able to launch weston. But with the bad performance.
What am I doing wrong or missing something?
Any help or advice would be appreciated! Thanks!
This is the dts file I have so far: stm32mp157c-odyssey.dts