Skip to main content
Visitor II
August 31, 2023
Solved

Issue with terminal output at putty with simple Helloworld program using Nucleo-L522ZE-Q.

  • August 31, 2023
  • 3 replies
  • 8675 views

 

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2023 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;

UART_HandleTypeDef hlpuart1;
UART_HandleTypeDef huart2;

RTC_HandleTypeDef hrtc;

PCD_HandleTypeDef hpcd_USB_FS;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC1_Init(void);
static void MX_LPUART1_UART_Init(void);
static void MX_RTC_Init(void);
static void MX_UCPD1_Init(void);
static void MX_USB_PCD_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ADC1_Init();
 MX_LPUART1_UART_Init();
 MX_RTC_Init();
 MX_UCPD1_Init();
 MX_USB_PCD_Init();
 MX_USART2_UART_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */

	 char buffer[]="Hello World\r";
	 HAL_Delay(100);
	 HAL_UART_Transmit(&huart2, (unsigned char *)&buffer, 6, sizeof(buffer));
	 HAL_Delay(1000);
	 HAL_GPIO_TogglePin (GPIOC, GPIO_PIN_7);
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE0) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure LSE Drive Capability
 */
 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_LSE
 |RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 55;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_MODE_INDEPENDENT;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_3;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief LPUART1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_LPUART1_UART_Init(void)
{

 /* USER CODE BEGIN LPUART1_Init 0 */

 /* USER CODE END LPUART1_Init 0 */

 /* USER CODE BEGIN LPUART1_Init 1 */

 /* USER CODE END LPUART1_Init 1 */
 hlpuart1.Instance = LPUART1;
 hlpuart1.Init.BaudRate = 209700;
 hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
 hlpuart1.Init.StopBits = UART_STOPBITS_1;
 hlpuart1.Init.Parity = UART_PARITY_NONE;
 hlpuart1.Init.Mode = UART_MODE_TX_RX;
 hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 hlpuart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 hlpuart1.FifoMode = UART_FIFOMODE_DISABLE;
 if (HAL_UART_Init(&hlpuart1) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&hlpuart1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN LPUART1_Init 2 */

 /* USER CODE END LPUART1_Init 2 */

}

/**
 * @brief USART2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{

 /* USER CODE BEGIN USART2_Init 0 */

 /* USER CODE END USART2_Init 0 */

 /* USER CODE BEGIN USART2_Init 1 */

 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */

 /* USER CODE END USART2_Init 2 */

}

/**
 * @brief RTC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_RTC_Init(void)
{

 /* USER CODE BEGIN RTC_Init 0 */

 /* USER CODE END RTC_Init 0 */

 RTC_PrivilegeStateTypeDef privilegeState = {0};

 /* USER CODE BEGIN RTC_Init 1 */

 /* USER CODE END RTC_Init 1 */

 /** Initialize RTC Only
 */
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = 127;
 hrtc.Init.SynchPrediv = 255;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }
 privilegeState.rtcPrivilegeFull = RTC_PRIVILEGE_FULL_NO;
 privilegeState.backupRegisterPrivZone = RTC_PRIVILEGE_BKUP_ZONE_NONE;
 privilegeState.backupRegisterStartZone2 = RTC_BKP_DR0;
 privilegeState.backupRegisterStartZone3 = RTC_BKP_DR0;
 if (HAL_RTCEx_PrivilegeModeSet(&hrtc, &privilegeState) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN RTC_Init 2 */

 /* USER CODE END RTC_Init 2 */

}

/**
 * @brief UCPD1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_UCPD1_Init(void)
{

 /* USER CODE BEGIN UCPD1_Init 0 */

 /* USER CODE END UCPD1_Init 0 */

 LL_GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* Peripheral clock enable */
 LL_APB1_GRP2_EnableClock(LL_APB1_GRP2_PERIPH_UCPD1);

 LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOB);
 LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOA);
 /**UCPD1 GPIO Configuration
 PB15 ------> UCPD1_CC2
 PA15 (JTDI) ------> UCPD1_CC1
 */
 GPIO_InitStruct.Pin = LL_GPIO_PIN_15;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = LL_GPIO_PIN_15;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /* USER CODE BEGIN UCPD1_Init 1 */

 /* USER CODE END UCPD1_Init 1 */
 /* USER CODE BEGIN UCPD1_Init 2 */

 /* USER CODE END UCPD1_Init 2 */

}

/**
 * @brief USB Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USB_PCD_Init(void)
{

 /* USER CODE BEGIN USB_Init 0 */

 /* USER CODE END USB_Init 0 */

 /* USER CODE BEGIN USB_Init 1 */

 /* USER CODE END USB_Init 1 */
 hpcd_USB_FS.Instance = USB;
 hpcd_USB_FS.Init.dev_endpoints = 8;
 hpcd_USB_FS.Init.speed = PCD_SPEED_FULL;
 hpcd_USB_FS.Init.phy_itface = PCD_PHY_EMBEDDED;
 hpcd_USB_FS.Init.Sof_enable = DISABLE;
 hpcd_USB_FS.Init.low_power_enable = DISABLE;
 hpcd_USB_FS.Init.lpm_enable = DISABLE;
 hpcd_USB_FS.Init.battery_charging_enable = DISABLE;
 if (HAL_PCD_Init(&hpcd_USB_FS) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USB_Init 2 */

 /* USER CODE END USB_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();
 HAL_PWREx_EnableVddIO2();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5|LED_RED_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(LED_GREEN_GPIO_Port, LED_GREEN_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, UCPD_DBN_Pin|LED_BLUE_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pins : PA5 LED_RED_Pin */
 GPIO_InitStruct.Pin = GPIO_PIN_5|LED_RED_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : UCPD_FLT_Pin */
 GPIO_InitStruct.Pin = UCPD_FLT_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(UCPD_FLT_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : LED_GREEN_Pin */
 GPIO_InitStruct.Pin = LED_GREEN_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LED_GREEN_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : UCPD_DBN_Pin LED_BLUE_Pin */
 GPIO_InitStruct.Pin = UCPD_DBN_Pin|LED_BLUE_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

 

raitaimoorali_0-1693514054813.png

raitaimoorali_1-1693514108650.png

Led is getting toggled but not getting anything at serial output. Please help. Thanks

 

    This topic has been closed for replies.
    Best answer by Tesla DeLorean

    >>I am not sure did i miss something? 

    The schematic and the user manual? You don't link to the tutorial, so no idea here if it refers to this board, or something else. The ST-LINK VCP has specific wired connectivity to a UART on the STM32L5, LPUART1 is the primary, and you'd have to change a lot of solder bridges to accommodate USART3 on PD8/PD9

    To use USART2 you need to wire the pins up to a USB-to-CMOS Serial adapter from SiLabs, FTDI, et al.

    3 replies

    Super User
    August 31, 2023

    What pins are you using? How are those pins connected to the PC? Can you open the port? What port are you opening? Do your port setting match?

    Note that the VCP is on USART3, not USART2.

    TeraTerm could also be buffering until it sees a "\n", but less likely.

    Visitor II
    September 1, 2023

    Hello @TDK 

    I have also tried to print hello world using USART3 but could not get at putty teraterm. I have attached the SS of all steps i have done please check. thanks

    raitaimoorali_0-1693580371991.png

    raitaimoorali_1-1693580388888.png

     

    raitaimoorali_2-1693580399253.png

    raitaimoorali_3-1693580411289.png

    raitaimoorali_4-1693580427692.png

     

     

     

     

     

     

    Graduate II
    August 31, 2023

    Hello @raitaimoorali 

    I suggest you first to use USART3 NOT USART2.

    Else,If PuTTY is not showing anything when you try to communicate with your STM32 board, there could be a few potential issues to consider:

    • Correct COM Port
    • Baud Rate
    • Bad Connections
    • USB Drivers problem 
    • Code Execution problem
    • Bad PuTTY Configurations

    If you've gone through these steps and are still encountering issues, it might be helpful to try a different serial monitor application or test the communication on a different computer to isolate the problem further.

    Best regards.

    II

    Super User
    September 1, 2023

    @Issamos  Are AI-generated responses really helping the forum here?

    Graduate II
    September 1, 2023

    What pins is it using? 

    Parameters here are all wrong.

     

    HAL_UART_Transmit(&huart2, (unsigned char *)&buffer, 6, sizeof(buffer));

     

    Try this

     

    HAL_UART_Transmit(&huart2, (unsigned char *)buffer, strlen(buffer), 500);

     

    Visitor II
    September 1, 2023

    Hello @Tesla DeLorean 

    Thanks for the reply i also tried your solution, but it did not work.

    for usart2

    PA2 = USART2_TX

    PA3 = USART2_RX

    for usart3

    PB10 = USART3_TX

    PB11 = USART3_RX

    but it did not work

    Graduate II
    September 1, 2023

    >>but it did not work

    How is USART2 supposed to be working in this context? How's it wired up that would facilitate this?

    Isn't the ST-LINK VCP connected via LPUART1 on PG7 and PG8 on the NUCLEO-L552ZE-Q ??

     /* Enable VddIO2 for GPIOG */
     HAL_PWREx_EnableVddIO2();
    
    //****************************************************************************
    
    void LPUART1_Init(uint32_t BaudRate) // LPUART1 TX1/RX1 PG7/PG8
    {
     GPIO_InitTypeDef GPIO_InitStruct = {0};
     UART_HandleTypeDef UartHandle = {0};
    
     __LPUART1_CLK_ENABLE();
     __GPIOG_CLK_ENABLE();
    
     /* UART RX/TX GPIO pin configuration */
    
     GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
     GPIO_InitStruct.Pull = GPIO_PULLUP;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     GPIO_InitStruct.Alternate = GPIO_AF8_LPUART1;
    
     GPIO_InitStruct.Pin = GPIO_PIN_7 | GPIO_PIN_8;
     HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
    
     /*## Configure the UART peripheral ######################################*/
     /* Put the USART peripheral in the Asynchronous mode (UART Mode) */
     /* UART configured as follow:
     - Word Length = 8 Bits
     - Stop Bit = One Stop bit
     - Parity = NO parity
     - BaudRate = 115200 baud
     - Hardware flow control disabled (RTS and CTS signals) */
     UartHandle.Instance = LPUART1;
    
     UartHandle.Init.BaudRate = BaudRate;
     UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
     UartHandle.Init.StopBits = UART_STOPBITS_1;
     UartHandle.Init.Parity = UART_PARITY_NONE;
     UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
     UartHandle.Init.Mode = UART_MODE_TX_RX;
    
     UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
    #ifdef UART_ONE_BIT_SAMPLE_DISABLE
     UartHandle.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
    #endif
    
     if (HAL_UART_Init(&UartHandle) != HAL_OK)
     {
     /* Initialization Error */
     Error_Handler(__FILE__,__LINE__);
     }
    }
    
    //****************************************************************************