kernel log "/cpus/cpu@0 missing clock-frequency property" on stm32mp151C
We are running a stm32mp151c with stm32mp linux built with yocto.
The kernel complain that the cpu0 clocl-frequency is not set, but the patch
layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp/5.10/5.10.116/0022-ARM-5.10.116-stm32mp1-r2.1-DEVICETREE.patch removes DTS clock-freuency setting
line 3889: - clock-frequency = <650000000>;
From release notes STM32 MPU OpenSTLinux release note - v4.0.0 - stm32mpu for 5.15 I found "BL2 always boots at 650MHz" and it seems the kernel should probe for cpu clock-frequency. The board boots, but we get these log entries that makes me wonder if we miss anything in DTS:
"Starting kernel ...
[ 0.003140] /cpus/cpu@0 missing clock-frequency property
[ 2.666366] stm32-cpufreq stm32-cpufreq: Failed to get chip info: -517"
Could anyone give me a hint where I can find more info about this patch and the background for removing the DTS cfg line "clock-frequency = <650000000>" but still code want to find DTS cfg please? I understand the opp should replace this but can both be used at the same time?