Let's Get Started - Garbage Serial Terminal Output
Hi,
I've been following the guide over at:
I'm using a Windows 10 as a host, but I was hoping I'm not the only one. I don't have access to a Linux environment at the moment.
I'm at the point where I need to connect to the device using the UART/ST-Link, power on, and press reset on the device to see an output on the terminal.
My setup is:
- Host is Windows 10
- Terminal is called Termite 3.4 (no install version)
- DK2 is powered from a dedicated USB power (500mA source)
- DK2 boots up fine (the display works and the demo environment seems to work ok)
- Serial settings I have as follows: COM3 9600 bps, 8N1, No Handshake
- 8 bits, no parity, 1 stop bit, no flow control
The output in the terminal, after pressing reset, is all jumbled and garbage:
[00] TÙ@¾"#V�Šÿ£[1B][18]Äã[12][07]€Åÿ‹3[15]"[03]ª�¢AÄ&KûÇÊ[0B]K[13]ÿ[05]ËœC[13]à ÕC BQpZ•®§#�qS‚[03]�?ƒˆJ##BÂ¥[05]ýÇõOEüc½½[08][1A]0Aáqú[07]¨ú[08]F[17][14]³³ÿÉ�?D±üðò…)E-Uÿ[1F]*ÿÀ[13][18]z�š™�?‘Ü¡"[1C]£ÑNâ„¢[11]$c{3�F†ý¡"M/ó‘çò1AÅ Xf$&WëÂ?4ýG¦ìGý�?3f`[13]+[16]m+nú�?3!¾…%!q�?0a >€rª €‘/•À.#Mé)[04]€@‘„�ò&Ù@^ó[00]‚7l-jO[00]"m¨MÑ%+�9¤ã/‚[16]§&36i9^[0B]õŸô[14]Ñ?F[0F]�?76'!‚‘+'„á#â‚.[13]#e[15]‚Óæâ#M+Aá.[13]#e[15]‚Óâá#Ä'[17]M©â3[02][15]È5Ñ¡†kAi+F¡¡Ù-'·B[08]&[17]M+‚¡!Ù-'§B[08]&[17]M##€FÙ«[10]m€3éE[19]Ä[13]M[1C]j?áIµ ÑÖ_Qt7DAF¤!e�±Çò3‰��?³¥3ùb M=Bá!&M-£[16]EÑu[00]F%#BE$N[08]Ñu§[02] �?€[04]M0e¡2�Ç‘�°�Rá[05]a�À[11]E�MƤ#€�¡ÂP[04]MÀ[07]Y�#%@� .Ú�[17]� Aiã7¦Mà [1D]#�‘[1D][16]\[15]’m$EêÛéÓ@�?Ô�?ێM+űeé%%ñÑÅ‘á#N[14][05]M+/ãke“t1-A[05][13]3 ±“M[02]†af�?â[14]‰‚+c0[0C]é[11]@©Â²[04][11]’Åâ#[03]$mIs©$¡m�?*B´g7éZ±M#a[17]'W#F f7Åán�áá[17]a©³É¡a[17]á°‚FŠÂa[17]6MM-%u3Ñ+©ÉcýWut•+ÑU�—mù[03]Ñ™3‚w�?§Ù[0F]m;Ã’'C^-Å¡+Â¥![07]‚fà ¨eÆ9,¦[0B]áÆ¶Â&-Ò°Ù†€ºU+B[1D][08]Æñ¦E�?[17]ÃN‘![12]¿á¢+ Å’[00]�?³F�?'�?á#=![12]»á¢#'Â¥WÃ_‘F�?'�?$#=![12]»}5æ'ÑF€ƒ¢æ7Ñ[08]±ñ¦e�?)[0B]»!À#%�?/áÒ¶#+¤ð#a�?_##MÂ@[17]ÂO-#uÑZ��+�úañ²„&aW-ö? Q'E°ñ[07]333[04]-N[02]á¡$[05]á#†Â[00][15]u„[06][11]á[02]ñ‚�[16]3#³[04]-'sa�'T;aÙ'3á[1B]Éa�g¢[1B];C¡#+çrr[0B]Æ'o ù—»O °“±m¥Ê06Ñ)_ åù?€G1D›Aá€f[13]ÂÇù‚^+[12]M|?Àã£ñ€Ñg&·�?¡‚#?@Jcùm'Sá+Ë¡áÂgñc>i[1D]+?âb[03]±'�?[06]"Aá/�?F
a™!‘c€}B�c+ÂF&[00]U¥'b[13]/¡%A±ñ_¨e##¥3 U#nQ2[00]MIGšW3Eñ‚À[06]á#3á3 Ô#f;"æà F#^ѧÿE¦Ñg9v3¹e[0F]M'[18]£ûEÃüMÓÿñÂ)
�?ûáW�?N7à “@�?6AÅ 7)[1B][1D]@F"±a™@ \ ó[08]i ?@‚o+]!Pë‘á 72[0F]uGÑx ± [17]+[00]m@Â6*X‚ÙƒM+u+Ü[17]ÒÛs�?[00]U)ò3[0B]ñi&[0C]ñáG³1‰ÓÛÙ/%_3>áÃñ!M5O31ùMO3q+áÒ6#[0F]²À£2¹M“Ʀ5Z�?fMáeÆ�[16]Ò&Õ&¥[13]ÙÒ0HM#Eå[15]&Kà ‰[17]#ÿ´@ÓŸt£[0E][05]á�Ù
6Ã[04]u<á ŒûÃ%À3�?B'ýðJ"æ
GgÿáÃ'ýÀEª[1E]GTÿÇC·�?Ã'
-Cáø�Ä»
ZÈý‚[0C]+¥
Ãêè=gìMÄq‚mg¥E&‘i÷€}@Ã�?ëÂ'uÃFn.øÀo¡Zñ´ù] 3¢£1ÿMefà âCÑ—„aÑevªGAað¡#=®[0B]mÂ&[03]M
AÄcÑax2J€mƒ„„ÿ†BÙg[16]“7'„·€ØÃ[02]$EG³1«‚“±a�?€�á“·³[16]ÂNMÃ,Va‘'![04]M&£¨¥v"DAé3[1B]‚’ðÉ Uá e“± ©%M/„aO%EÂO�?Â?ÖÂãÂEóm×/™á‚þ-Ê3�?�?7�?A[15]3
M9¡‚F¼¡FW=5@�?y¦©Má„'�?Y[17]M/fQ.[13]“?‰÷MÔá[0E]-Vé/�?^Ñ´©}7e‡L¦MÔñÈ"€fQee+¥Æa‘ò£-FEE†�?�?[13][1A]ö�?Aæã$[07]�?;FD¦4a[16]L+[02][15]%óD´¥M;F4[03]€ü�[13]‚±‚üE �?"[00]M¡Ÿ3¶r†Ä�?[00]À"[03]‚ ‡LæÀÄá2£áe?uU[„‚8¢²[19]]†‘’'=o�?†‰�? ~ìüm'#Ma[07]éÌ«¡ayrsca�?á'¥´%H&9[05]mDÂD#�ðMG[0B]^OÔ�,Wå��ñ¿¢BAáçñ[14]ñÂÓ<’?jaÂÙ#MM[0E]�?1_À[0B]c£�?õ[05]+[08]E[17]ê[17]Óš‰0[10]B2[0F][01]CÙn[00]²7ùm!ò™…è;K+&æd£[02]ðÂ@7Ÿ]ê[0B]Ù_[00]MS'F€[0B]D£#¯�?áÅ…-S�?y#“[13]Bû¡KÀéqn üÂà ª#<ð�[~ÿM&Ç‘ $M1�?[Fv�?÷Âà ®Ó†.ÿ[15]R[�áF6ªüFv±�-#ÀFvéHà Ff¡˜ëF¶ª#77ÿ-¦£ÀÿÖ[16]Ù«¦[05]"/ÿO¦ˆòPvÀ�?ÿ�?¾Ë‡ý[00]7¡[10]?€¾&ù�?ÉÅý€/3ûV6à >ž[10]u€ÿÀÉ[0F]Ã][07]‘·[1C]éb#f[1C]v[04]F6à #e~ü[05]"[1F]ÿ-Ü„ÙÃ[15]R2[07][05]B[07]&ý-R«Å�>ãÖ
ž]—bËÿ- à ÿ[05]FQ÷[05]B&k#"cÿPÀ›�?[06]&›[1D]3Ö\*[1F]ÿ[10]O£%ÿO[04]+&F¦2�ÿ[05][02]&¦ýFvˆ„»[15]R¢-'€^Ã.%[06]°O£ˆŸ�/&Vö¨ßà 6ãÆ�?á'¢—·Êÿ[00]'[01]óÿ-ܾ�?�Vvø÷[10]U»ÿVVñ‘ÖV�?¸€6ãÖ5l]—bËÿF¦.›[05]"?¢ü[02]gæe[05]Fâ„¢3Ô[10]M#ÖùM§ùÖV‘Ì=ÿ-\[0E]s[15]2§LÓ‚I# `ÃÿF6Èã=†*g¿O[04]>#O¤�?j#ðáÒü[17]Ê3ü[10][0E][07]¦ÙV[17][14]Ã…A3[06]]ÿ�?†HcqáØgÿ-R[1B]È%&%#€vA#ü€N[08]Â?³Ú�?’%+qþè_+üM‘õV6[07].=&�[1F]+÷ÖÖ¹ô}%‚aÇC/añBt�?%e�?�?F¶ª-ÖFIµ]Y¶ÂÂÆÿF¦ªÒ[10]}é�?ÉÂ�?òܰTÿP�æ-ýÜ4ÿÖF+³*'ñM#�O'M&ÿƒB4±¦[02]7jÿP�?ùF6à û�?VL#Y[07]ñ=†&
ÿb²'[03]d¨ã�Y¢[15]Rº£óᑣ»7ÿMPT© ¹Uqˆ^ó[05]BƒùÑDÂ#1/¢ðÔ[0E]wú[15]B.ÿÄ £Ò-à u�?„�?á‹€F[04]�?ÂX�?[1A]âÉÿÃ6ãc[05][02]"¯ÅéÄ=†"Ƶ÷[05]B;�ùf[06]!·ž´·vfMg[05]ý[1E]Ó¾vO'Ž4¦…–@³Ž-ý“e-Ig-ý£†-[15]3.}ÿ³e‚#�4Y†c%7Ž4±ÓvM'-ý[00]g„ýÖ[16]Ç7!§[10]n®;@+}ÿF6ÈÆÂùÜÀ@%¸¡ý[05][02]®ÿ[05]B/�?à [05][02]*8��?�?ÿF6Àß[00]7Ÿ-£ü[10]U³6F¶ªÚ[00]·*ÿÖF*û[15]RŽùÖF.ÿ[00]7.ÿ[00]'.?øVVÑù[05]B®ä-[06]*üÖF"ÿ
Àô[00]§>J[00]§Èé_$ÀNýF6°\[05]B§'ŠVVAùÿVVAÿ[15]Ró%ÖÖ¹[06]F¶ªÂÿ[10]N£ÀýÖF'ó…ÿ[1B]Àð-’5ƒ/wýd][1F]‡ñ7ÿHas anyone got any tips for me at this point? Any settings I should be going over? I tried looking over the guide, but I don't think the settings were referenced anywhere for the serial connection.
Best regards,
Tero