libqmi build for STM32MP157
I'm building libqmi for the STM32MP157 and getting an error at this point in the build
GISCAN Qmi-1.0.gir
Traceback (most recent call last):
File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/bin/g-ir-scanner", line 98, in <module>
from giscanner.scannermain import scanner_main
File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/gobject-introspection/giscanner/scannermain.py", line 35, in <module>
from giscanner.ast import Include, Namespace
File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/gobject-introspection/giscanner/ast.py", line 29, in <module>
from .sourcescanner import CTYPE_TYPEDEF, CSYMBOL_TYPE_TYPEDEF
File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/gobject-introspection/giscanner/sourcescanner.py", line 34, in <module>
from giscanner._giscanner import SourceScanner as CSourceScanner
ImportError: /home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/gobject-introspection/giscanner/_giscanner.cpython-310-x86_64-linux-gnu.so: wrong ELF class: ELFCLASS32
make[4]: *** [/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/share/gobject-introspection-1.0/Makefile.introspection:156: Qmi-1.0.gir] Error 1
So it has a problem with _giscanner.cpython-310-x86_64-linux-gnu.so: wrong ELF class: ELFCLASS32
Any idea why?