Linux-console on UART for STM32MP25 / STLinux
Hi,
for evaluation I'm running STLinux on a STM32MP257F-DK board currently.
I found the Linux console is available on one of the USB-ports with the default configuration of that operating system.
Quick question: is that Linux console also available on some plain UART-port for that development kit (or for the STM32MP25 in general)? If yes: which port is used?
Thanks!