Low Power MPU For Connecting 2 Cameras, Several Peripherals, OTA Updates
Hello, all!
For some time now I have been trying to come up with a solution to connect 2 cameras of 480X640 resolution and several peripherals to a low-power MCU.
I keep hitting a wall, because it seems that this endeavor is not suitable for an MCU - the large RAM required to host 600K image, the fact that I can't connect 2 USB / DCMI cameras and need several MCUs that defeat the purpose, the fact that having a DCMI, an FSC and several peripherals on the same MCU, that is also, low-power, is unheard of..
So, I'm trying my luck with an MPU:
- does ST offer a low-power MPU that has a large RAM, >100 IOs, and most importantly - can interface 2 USB cameras?
- Is there a tool like MCU FInder for MPUs?
- Are there guides for getting strated with ST MPUs?
- Is it possible to perform an Over The Air Update with an ST MPU?
Thanks!
** Partial answers will be much appreciated as well. Just starting off with the MPU direction, and want to understand if it suits my needs and how challenging it would be.