modify a CAN sample point
I using a STM32MP-157F-EV1 eval board with linux Version 4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.
CAN receive 500kBit/s fails, if I modify the sample point via an console command it works well. All other Bitrates 125kBit / 250kBit 1MBit are ok with the default values.
How could I set the sample point permant, is there a linux config-File, to get the modyfied value even after a reboot?