Question
Moving LTDC pins on DK2 board?
Just wondering if I can edit the pinctrl.dsi file to change the pins to the Raspberry Pi header, rather than the HDMI encoder, so I can try DPI Raspberry Pi displays.
In CubeMX the LTDC and most of the peripherals are locked, just wondering if it is necessary to configure them there or if a device tree configuration is enough.
Thanks