Skip to main content
Visitor II
December 17, 2025
Question

Need a support to probe TC358743 (HDMI to CSI ic)

  • December 17, 2025
  • 0 replies
  • 158 views

I am trying to probe TC358743 (HDMI to CSI ic) to STM32MP257f-dk. The ic is able to take input from the HDMI from my laptop (I is being checked as when i give an edid as input from v4l2 then the screen of my laptop gets extended).

The problem is in receiving the stream at stm32. TC358743 outputs 2 formats - MEDIA_BUS_FMT_RGB888_1X24 and MEDIA_BUS_FMT_UYVY8_1X16. Both of them are not supported by CSI input of stm.

    This topic has been closed for replies.