Skip to main content
Graduate
April 12, 2022
Question

No package 'wayland-client-protocol' found !

  • April 12, 2022
  • 5 replies
  • 1688 views

Hello ,

I am building one application using Open gl es code. but gettign this error.Not sure if it is error as the final applications is building fine but giving error while elaunching .

No package 'wayland-client-protocol' found

Finished building target: my application

on launching this application it gives :

========== init_wayland_system ==========

Error : No such file or directory

can't connect to wayland display

========== init_wayland_system ==========

WHats happening here?

Regards,

D

    This topic has been closed for replies.

    5 replies

    Technical Moderator
    April 14, 2022

    Hello @darla14​ ,

    Could you please give me a little bit more information concerning your issue ?

    • Are you using Distribution or Developer package to make your application ? (If Distribution, with which OpenSTLinux version ?)
    • Is it possible to share us your source code to replicate from our side ?

    Regards.

    Erwan.

    darla14Author
    Graduate
    April 19, 2022

    Hello @Erwan SZYMANSKI​  ,

    thanks for the reply,

    I cross-compiled the application using the mpu toolchain ( in sdk) for the starter package I flashed,. It has some code that runs on the gpu.

    Difficult to share sc ...but i will check..

    what issue do you see?

    Br,

    Technical Moderator
    April 22, 2022

    Hello @darla14​ ,

    sorry for late answer, are you still blocked ?

    Ok no problem for the SC, can you share me your Makefile or your compilation options (CCFLAGS, LDFLAGS etc..) with masking sensitive information if there are ?

    Rgs.

    Erwan.

    Technical Moderator
    April 22, 2022

    Moreover, do you have a weston service running when you try to execute your command ?

    As far as I remember, using OpenGL ES with wayland-egl library needs it.

    Regards.

    Erwan.

    darla14Author
    Graduate
    April 22, 2022

    Thanks @Erwan SZYMANSKI​ 

    Let me check on all these points and come back !

    Br,

    Technical Moderator
    June 9, 2022

    Hello @darla14​ ,

    Do you still need help on this issue?

    Regards,

    Kevin

    darla14Author
    Graduate
    June 9, 2022

    Not now,thanks for the comment . @Kevin HUBER​ 

    Regards,