NTP Syncronization using STM yocto BSP.
Hi,
I have STM32MP157C-DK2 demo board and I have ported STM Linux Yocto into board. I have enable NTP in the bb layer and I am able to see the NTP is up. When I want to get the status using timedatectl status I am getting the following output
Local time: Wed 2019-10-30 15:16:43 UTC
Universal time: Wed 2019-10-30 15:16:43 UTC
RTC time: Wed 2019-10-30 15:16:44
Time zone: n/a (UTC, +0000)
System clock synchronized: yes
NTP service: active
RTC in local TZ: no
Where we can find that NTP service is active but the time zone was not able to find. Defaultly it was taking UTC time zone.But I want to change the time zone to Asia/Kolkata.
So, I need to support for changing the timezone to Asia.
Regards
Srikanth.