Hello @ANalg.1 ,
The software framework needed to make the murata 1DX works is only available under linux (A7Core).
As specified on the wiki related to WLAN: https://wiki.st.com/stm32mpu/wiki/WLAN_and_Bluetooth_hardware_component#Software_frameworks
Regarding the hardware assignment of the peripheral and its DT configuration, you can see in the following link, that the brcm node is defined in the node sdmmc2:
https://wiki.st.com/stm32mpu/wiki/WLAN_device_tree_configuration#DT_configuration_-28board_level-29
It is explained in the Peripherals overview page that sdmmc2 is CortexA7 only:
https://wiki.st.com/stm32mpu/wiki/STM32MP15_peripherals_overview#Internal_peripherals_overview
So you can't use the module muRata 1Dx with core-M4 only.
Hope it helps,
Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'