On VMWare's Ubuntu 20.04 LTS, the STM32 program tool is not associated with the STM32MP157D evaluation board.
Hello, teachers.
First, The board I am using is the STM32MP157D evaluation board.
I checked the article that the starter package can be installed in Windowsos, but the developer package and the distribution package are only available in the Linux environment.
In addition, Ubuntu 18.04 was installed on VMware as Ubuntu 20.04 LTS because it may not be compatible.
I installed the virtual environment and the STM32Cubeprogrammer Tool, and I tried to connect with virtual Linux by booting the board in USB mode, but the STM32 tool on Linux cannot find it.
By installing another USB device on the PC, we confirmed that the USB driver works normally.
The STM32Cubeprogrammer version is seen as API v2.12.0 | Linux-64bits.
How can I connect to the STM32MP157D-EV1 board and USB in a VMWare Linux environment (Ubuntu 20.04 LTS)? Please give me a hint.