Skip to main content
Visitor II
January 13, 2021
Question

OpenAMP compilation with cpp

  • January 13, 2021
  • 4 replies
  • 1239 views

i am trying to compile the third party OpenAMP folder in IAR with C++ and am facing a lot of errors.

how can these be resolved.

0693W000007B5ZuQAK.png

    This topic has been closed for replies.

    4 replies

    Technical Moderator
    January 19, 2021

    Hi @SMang.1​ 

    Which version of ecosystem are you using ?

    CubeMX version ? Firmware package ?

    Thanks

    Olivier

    Visitor II
    August 31, 2021

    Hello,

    I am facing a similar issue. If i keep my main file with .c extension it works, but except for the generated code, we have entire code base in cpp.

    Can you please help

    Technical Moderator
    September 1, 2021

    Hi @JTari.1​ ,

    This remind me limitation we got in old version ecosystem V1 :

    https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/STM32CubeMP1_Package_release_note_-_v1.1.0#Known_issues_and_limitations

    But their are no more mention in last V3.

    So it should works using latest CubeMP1 package V1.4.0

    Did you generate your project with CubeMX ?

    Did you check if provided exemple in Cube Package are working ?

    STM32Cube_FW_MP1_V1.4.0\Projects\STM32MP157C-DK2\Applications\OpenAMP\OpenAMP_raw

    STM32Cube_FW_MP1_V1.4.0\Projects\STM32MP157C-DK2\Applications\OpenAMP\OpenAMP_TTY_echo

    Olivier

    Visitor II
    September 1, 2021

    Hello,

    Thankyou for the reply. i am not using MP1 package but STM32H7 package for dual core microcontrollers. Yes i used the CubeMX to generate the code.

    The problem arises because of using c++ instead of c. I guess OpenAMP doesnt support c++. Is there any help on this?

    Technical Moderator
    September 1, 2021

    Hi, you mean you work on H7 platform ?

    In that case worth to open a new post in STM32H7 community.

    Olivier