OpenAMP Linux Side
Hi,
iam trying to get an understanding of the OpenAMP Framework and i wanna use it for interprocess communication with the STM32MP1. As my understanding, the OpenAMP Framework could be used from Baremetal/RTOS side and apparently also from Linux Side. But when i had a look to the stm-wiki site i only found an Implementation of the OpenAMP to the Cortex M4 not to the A-Cores. So my question is, if there is any example to use OpenAMP also on the A-Cores, with the STM32MP1. Another Question is, if its possible to run the Linux in Slave Mode and the M4 In Mastermode? In my understanding its not possible with the STM32MP1 or?