Skip to main content
Visitor II
June 19, 2023
Question

OpenSTLinux SDK Manager can't find updated SDK

  • June 19, 2023
  • 1 reply
  • 1076 views

Hi 

I have used the "bitbake -c populate_sdk st-image-weston" command to generate an updated SDK with OpenCV and ZerMQ packages. The SDK is generated successfully.

The issue is when I want to use this SDK in STM32CubeIDE, since I can't seem to find the SDK in "OpenSTLinux SDK Manager" under Window ==> Preferences. The manager can easily find the standard SDK which can be downloaded from the website. 

I suspect the issue to be the version name, since the updated SDK outputs "4.0.4-snapshot" instead of "4.0.4-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23" when entering:

PC >> echo $OECORE_SDK_VERSION

What can I do to fix this? :)

(OpenSTLinux SDK Manager unable to see SDK)

MarcusRJ_0-1687161319965.png

(Updated SDK folder)

MarcusRJ_1-1687161359883.png

 

 

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    June 29, 2023

    Hi @MarcusRJ ,

     

    In order to be seen by "SDK manager"  SDK version might contain "openstlinux-" 

     

     

    Hope it help 

     

    Olivier