optee 3.12, stm32mp1 custom board and DRAM (256M) sizes.
I have a custom board with a stm32mp151c and 256M DRAM.
Trying to get optee 3.12 from ecosystem 3.0.0 to start.
Everything works fine with tf-a 2.4-r1 and sp_min, u-boot 2020.10 etc.
But I can't get optee to start. I've enabled a high loglevel and the last print I get from optee is:
...
I/TC: Pager is enabled. Hashes: 2208 bytes
Then everything goes quiet. No stacktrace, fault, or anything else. Just "dead".
To me, this looks like some very basic issue with DRAM sizes etc. But I can't say for sure.
My dts looks correct with memory regions and declarations.
But I noticed that in the build conf.mk was getting some weird stuff.
CFG_DRAM_SIZE
CFG_SHMEM_START
CFG_TZDRAM_START
These three had some wonky values for a 256M board. And they seem to be used?
So my conclusion is that it does not suffice to set dts properties for optee, some tweaking of platform memory sizes (looks like there are options for 512M 1G etc, but not 256M) needs to be done.
Anything else that needs to be fixed for a 256M board?
Maybe this information can be valuable to someone with a custom board.