Skip to main content
Visitor II
December 25, 2024
Question

OSTL V4.1.2 u-boot, TF-A not displaying correct version while boot up

  • December 25, 2024
  • 0 replies
  • 604 views

Using OSTL 4.1.2 and build DISTRO=openstlinux-weston MACHINE=stm32mp15-disco on STM32MP157F-DK2. Found that while boot up serial console showing incorrect version of  u-boot and TF-A. 

Although kernel version is correct i.e. 5.15.145.

TF-A : v2.6-stm32mp1-r2.1(debug):v2.6-dirty(a1f02f4f)

u-boot: U-Boot 2021.10-stm32mp-r2.1 (Oct 04 2021 - 15:09:26 +0000)

This should be v2.6-stm32mp1-r2.2 and 2021.10-stm32mp-r2.2.

Following are messages while boot up

1. NOTICE: BL2: v2.6-stm32mp1-r2.1(debug):v2.6-dirty(a1f02f4f)

2. optee optee: OP-TEE: revision 3.16 (d0b742d1)

3. U-Boot 2021.10-stm32mp-r2.1 (Oct 04 2021 - 15:09:26 +0000)

 

4. ## Booting kernel from Legacy Image at c2000000 ...
Image Name: Linux-5.15.145
Created: 2023-12-23 9:42:00 UTC

I am using STM32 MPU OpenSTLinux release note - v4.1.0 - stm32mpu-ecosystem-v4

  • New manifest tag available to get the release: openstlinux-5.15-yocto-kirkstone-mp1-v24.07.17
repo init -u https://github.com/STMicroelectronics/oe-manifest -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v24.07.17
repo sync

 

Do you have patch to print correct version bootup console?

 

    This topic has been closed for replies.