"pip3 install ***" error
hi st expert
When i use pip3 install some package on board, i get some error as follew:
running build_ext
building '_cffi_backend' extension
creating build/temp.linux-armv7l-3.8
creating build/temp.linux-armv7l-3.8/c
arm-ostl-linux-gnueabi-gcc -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a7 -Wno-unused-result -Wsign-compare -DNDEBUG -
g -O3 -Wall -O2 -pipe -g -feliminate-unused-debug-types -fmacro-prefix-map=/python3/3.8.2-r1=/usr/src/debug/python3/3.8.2-r1 -fdebug-prefix-m
ap=/python3/3.8.2-r1=/usr/src/debug/python3/3.8.2-r1 -fdebug-prefix-map== -fdebug-prefix-map== -O2 -pipe -g -feliminate-unused-debug-types -f
macro-prefix-map=/python3/3.8.2-r1=/usr/src/debug/python3/3.8.2-r1 -fdebug-prefix-map=/python3/3.8.2-r1=/usr/src/debug/python3/3.8.2-r1 -fdeb
ug-prefix-map== -fdebug-prefix-map== -fPIC -DFFI_BUILDING=1 -I/usr/include/ffi -I/usr/include/libffi -I/usr/include/python3.8 -c c/_cffi_back
end.c -o build/temp.linux-armv7l-3.8/c/_cffi_backend.o
unable to execute 'arm-ostl-linux-gnueabi-gcc': No such file or directory
error: command 'arm-ostl-linux-gnueabi-gcc' failed with exit status 1
[end of output]
note: This error originates from a subprocess, and is likely not a problem with pip.
error: legacy-install-failure
could you give me some advice for this issue? thanks
B&R
Tao