Playing Video with gst-launch
Hi,
I want to play a video from mounted USB stick. Once USB plugged the host, I mount it with "mount /dev/sda1 /mnt" and than quit the psplash screen with "psplash-drm-quit" on target. After that, trying to play a video with "gst-launch-1.0 playbin uri=file:///media/aaa.mp4" but there is nothing screen on TFT. Also, I have tried this "gst-launch-1.0 v4l2src ! "video/x-raw, width=1280, Height=720, framerate=(fraction)15/1" ! queue ! autovideosink -e" command but there is nothing again.
Console Output;
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
WARNING: from element /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0: Could not open DRM module (NULL)
Additional debug info:
../../../gst-plugins-bad-1.14.2/sys/kms/gstkmssink.c(709): gst_kms_sink_start (): /GstKMSSink:autovideosink0-actual-sink-kms:
reason: No such file or directory (2)
Setting pipeline to PLAYING ...
New clock: GstSystemClockFurthermore, I have tried camera examples for qt it too can't playing video or not seen on TFT altough the path of video has been selected right . Also, why is the landscape of TFT wrong and width/height of screen? I can't see the application fullscreen.