Skip to main content
Visitor II
December 17, 2019
Solved

problems with installing fftw package

  • December 17, 2019
  • 1 reply
  • 1471 views

Hi! Have some problems with installing fftw package. I tried to install it to st-image-weston and st-example-image-xfce, but received same error when bitbake run do_rootfs. Can anybody explain this problem?

Build Configuration:

BB_VERSION          = "1.40.0"

BUILD_SYS           = "x86_64-linux"

NATIVELSBSTRING     = "universal"

TARGET_SYS          = "arm-openstlinux_x11-linux-gnueabi"

MACHINE             = "stm32mp1"

DISTRO              = "openstlinux-x11"

DISTRO_VERSION      = "2.6-snapshot-20191213"

TUNE_FEATURES       = "arm armv7ve vfp thumb neon vfpv4 callconvention-hard cortexa7"

TARGET_FPU          = "hard"

DISTRO_CODENAME     = "thud"

ACCEPT_EULA_stm32mp1 = "1"

GCCVERSION          = "8.%"

PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"

meta-python          

meta-oe              

meta-oe              

meta-gnome           

meta-xfce            

meta-initramfs       

meta-multimedia      

meta-networking      

meta-webserver       

meta-filesystems     

meta-perl            

meta-python         

meta-st-stm32mp      

meta-qt5             

meta-st-openstlinux  

meta                = "master:364b6270b0787afe634252406c4c559ba592b6a3"

workspace           = "<unknown>:<unknown>"

meta-qt4            = "master:ec8e0800ef1c33b72f3d3924412dabc48c2a55ac"

Initialising tasks: 100% |###########################################################################################################################################################################| Time: 0:00:13

Sstate summary: Wanted 448 Found 442 Missed 6 Current 3139 (98% match, 99% complete)

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: st-image-powmach-1.0-r0 do_rootfs: Unable to install packages. Command '/home/vlad/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/build-openstlinuxx11-stm32mp1/tmp-glibc/work/stm32mp1-openstlinux_x11-linux-gnueabi/st-image-powmach/1.0-r0/recipe-sysroot-native/usr/bin/apt-get install --force-yes --allow-unauthenticated apt dpkg packagegroup-base-extended packagegroup-core-boot packagegroup-core-eclipse-debug packagegroup-core-ssh-dropbear packagegroup-core-tools-profile packagegroup-core-x11 packagegroup-framework-core packagegroup-framework-core-base packagegroup-framework-sample-xfce packagegroup-framework-tools packagegroup-framework-tools-base psplash-drm resize-helper run-postinsts systemd-mount-partitions xf86-video-modesetting' returned 100:

Reading package lists...

Building dependency tree...

Reading state information...

Some packages could not be installed. This may mean that you have

requested an impossible situation or if you are using the unstable

distribution that some required packages have not yet been created

or been moved out of Incoming.

The following information may help to resolve the situation:

The following packages have unmet dependencies:

packagegroup-framework-sample-xfce : Depends: fftw but it is not installable

E: Unable to correct problems, you have held broken packages.

ERROR: st-image-powmach-1.0-r0 do_rootfs: Function failed: do_rootfs

ERROR: Logfile of failure stored in: /home/vlad/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/build-openstlinuxx11-stm32mp1/tmp-glibc/work/stm32mp1-openstlinux_x11-linux-gnueabi/st-image-powmach/1.0-r0/temp/log.do_rootfs.28752

ERROR: Task (/home/vlad/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-powmach.bb:do_rootfs) failed with exit code '1'

    This topic has been closed for replies.
    Best answer by KnarfB

    How did you try to add this package to the image? There is a subtle difference between recipe names and package names. The fftw recipe can build a package named libfftw, see fftw_3.3.6.bb. Try to add libfftw to your image.

    hth

    KnarfB

    1 reply

    KnarfBAnswer
    Super User
    December 18, 2019

    How did you try to add this package to the image? There is a subtle difference between recipe names and package names. The fftw recipe can build a package named libfftw, see fftw_3.3.6.bb. Try to add libfftw to your image.

    hth

    KnarfB