Question
QEMU on stm32mp157
I want to emulate the stm32mp157 on qemu. I have been taking the kernel image and initrd from yocto build, but it is not loading the kernel. using the following command
qemu-system-arm \
-M virt -smp 8,sockets=1,cores=4,threads=2 -m 4G \
-cpu cortex-a7 \
-device virtio-tablet-pci \
-device virtio-keyboard-pci \
-device virtio-net-pci,netdev=net0,mac=52:54:00:12:34:02 \
-device virtio-gpu-pci \
-device virtio-rng-pci,rng=rng0 \
-netdev tap,id=net0,ifname=$TAP,script=no,downscript=no \
-object rng-random,filename=/dev/urandom,id=rng0 \
-serial mon:stdio -serial null -nographic \
-initrd senecos-image-stm32mp1-ems-c2-faa1-20230803140050.rootfs.cpio.gz \
-kernel Image \
-append 'root=/dev/ram0 rw debugshell ip=192.168.7.2::192.168.7.1:255.255.255.0::eth0:off:8.8.8.8 console=ttyAMA0 console=hvc0 '