QSPI Clock Question
Hi,
Is there a way to set the QSPI clock on the MP157 to be free running while also using the QSPI? The programming manual mentions that free running mode will prevent the QSPI from being usable.
I am working on a project to interface the MP157 to an FPGA via QSPI, however, having the clock start up only when the transaction is active prevents the QSPI clock from being able to drive an IO PLL. If it were free running when no transaction was active, then the FPGA could maintain a synchronous PLL lock on the MP157.