Qt SDK build failed
Hi All -
I was attempting to build the Qt example images for the DK2, following the wiki directions here:
https://wiki.st.com/stm32mpu/wiki/How_to_build_and_use_an_SDK_for_QT
I got to the step where it's building the SDK, after compiling the image successfully.
PC $> bitbake st-example-image-qt -c populate_sdk
And got a compile error:
arm-ostl-linux-gnueabi/9.3.0/ld: .obj/moc_qgeotiledmaplabs_p.o:(.data.rel.ro+0x70): undefined reference to `QGeoTiledMap::setCopyrightVisible(bool)'
| /home/mtd/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtlocation/5.14.2+gitAUTOINC+feb604c326_d9577fdebe-r0/recipe-sysroot-native/usr/bin/arm-ostl-linux-gnueabi/../../libexec/arm-ostl-linux-gnueabi/gcc/arm-ostl-linux-gnueabi/9.3.0/ld: .obj/moc_qgeotiledmaplabs_p.o:(.data.rel.ro+0x80): undefined reference to `QGeoTiledMap::clearScene(int)'
| /home/mtd/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtlocation/5.14.2+gitAUTOINC+feb604c326_d9577fdebe-r0/recipe-sysroot-native/usr/bin/arm-ostl-linux-gnueabi/../../libexec/arm-ostl-linux-gnueabi/gcc/arm-ostl-linux-gnueabi/9.3.0/ld: .obj/moc_qgeotiledmaplabs_p.o:(.data.rel.ro+0x84): undefined reference to `QGeoTiledMap::evaluateCopyrights(QSet<QGeoTileSpec> const&)'
| collect2: error: ld returned 1 exit status
| make[2]: *** [Makefile:774: ../../lib/libQt5Location.so.5.14.2] Error 1
| make[2]: Leaving directory '/home/mtd/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtlocation/5.14.2+gitAUTOINC+feb604c326_d9577fdebe-r0/build/src/location'
| make[1]: *** [Makefile:181: sub-location-make_first] Error 2
| make[1]: Leaving directory '/home/mtd/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtlocation/5.14.2+gitAUTOINC+feb604c326_d9577fdebe-r0/build/src'
| make: *** [Makefile:49: sub-src-make_first] Error 2
| WARNING: exit code 1 from a shell command.
|
And this summary:
Summary: 1 task failed:
/home/mtd/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/layers/meta-qt5/recipes-qt/qt5/qtlocation_git.bb:do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
Help?